Front of line to end of line, our sensors, grippers, carbon fiber components, finger tooling and suction cup solutions lead the industry.
We are the intelligent handlers that move parts through space to make your metal stamping operations world-class.
Our expertise in tri-axis, crossbar and tandem press line material handling is unparalleled.
We want you to have the resources you need to help you select and order the best products, quickly and efficiently.
We are proud of our long history, and the same entrepreneurial spirit that drove our founder is still alive today, driving our continued focus on innovation and excellence.
Missing studs and studs with missing threads can mean thousands of dollars lost in scrap and time spent hand sorting. Our stud sensors are a technological leap forward, and help prevent delays and reduce the cost of quality control during sheet metal fabrication.
Quality Checking: Are you trying to use an off-the-shelf sensor to detect whether a stud is present or not or whether it has threads? It’s a little late to learn that a stud has no threads when you’re trying to bolt an assembly together. Our inductive stud thread detector is the only sensor engineered to be sensitive and reliable enough to detect threads, so you’ll never again send a welded piece through to assembly with a faulty stud.
Harsh Environments: Every time a stud touches a sensor, the threads act like a file, slowly wearing the housing and faceplate away, unless of course, that sensor is our stud thread detector. With all steel housings and faceplate, this detector stands up to rigorous use. And we have mastered the art of keeping the steel sensor tuned. Not every steel sensor can do that.
Heavy Side Loading: Automation is precise and repetitive, but it’s not always perfect. Sometimes a part comes down on a sensor just enough out of place to impact the sensor. This can damage or wear out an ordinary sensor, but not the stud thread detector. The stainless steel construction stands up to heavy side loading, and it won’t gouge the threads either.
The NSS stud thread detector can detect M5, M6, M8, and M10 studs or thread presence, and is great for heavy duty or weld applications.
Compatible with the NSS0506 Stud Sensor, the spring mount allows the sensor to retract when the stud is out of place.
Complete with LED lighting for on/off status of sensor, the monitor for the SNS series nut sensor has an interface that is directly programmable to controllers.
Norgren's compatible sensor cables have 3-Pin PICO connections, and come in straight and right angle connector styles.